You may have a choice of several different physical interfaces with which to connect your instrument to your computer. This topic will give you some guidelines to help with that decision. If you are constructing a large or complex test system, or if your test system will be used for a long time, you will want to make this decision carefully.
First, determine the interfaces that are available to you on each side of the connection (instrument and computer). Not all interfaces are available on all instruments. Computers typically have USB, LAN, and a limited number of serial (RS-232) interfaces available, but require the addition of an interface card (such as the Keysight 82350B PCI GPIB Card) to support GPIB.
Adaptor products are available to connect a computer to GPIB instruments using either the computer's USB interface (Keysight 82357B USB/GPIB Interface Converter) or its LAN interface (Keysight E5810B LAN/GPIB/USB Gateway). These products provide convenient and powerful ways for you to take advantage of computer-standard IO with a large range of instruments.
A local area network (LAN, also known as Ethernet) provides instrument connectivity over distances and allows sharing of instruments among multiple users and multiple computers. Ethernet LANs are almost universally available; they support data rates of 10 MB/second to 1 GB/second and they use inexpensive cables and connectors. Many instruments have LAN interfaces built in. For those that do not, you can use the Keysight E5810B LAN/GPIB/USB Gateway). LAN is a recommended method to connect instruments together in applications such as new test systems.
You can connect your instruments to a private LAN or to a site LAN.
When you are connecting a new instrument to your network (private or site LAN), you have several options. Click the links below for more information.
In order for BenchVue to recognize and communicate with a PXI modular instrument, you must first enable the HiSLIP interface from the instrument's Soft Front Panel (SFP). For more information, see Connecting to PXI Modular Instruments.
The Universal Serial Bus (USB) is a quick and easy way to connect instruments to computers. Some newer instruments have USB interfaces built in. For those that do not, you can use the Keysight 82357B USB/GPIB Interface Converter to establish connectivity easily and inexpensively. You can one USB port to connect a single instrument to a PC; or, via the 82357B, you can connect up to 14 GPIB instruments to one USB port.
Note: If you are using USB to connect to your instruments, make sure you are using USB 2.0 ports. At this time, you might experience connection integrity and performance issues with USB 3.0 (indicated by "SS" next to USB connector on computer).
The General Purpose Interface Bus (GPIB) is fast and robust, but requires a special PC card and additional configuration steps. Many existing systems are based on GPIB, and it is the best option for many instruments that have only GPIB and serial connectors.
Serial connection is inexpensive and widely available, but is slow compared to other I/O interfaces, and requires particular attention to cabling and configuration. Instruments connected via serial port are not normally automatically detected by I/O software. Connect your instruments via serial port only if these factors are not a concern for you, or if no other option is available.